DIN#.FILTER
Description
This parameter gets or sets the digital input filter. The digital filter blocks input changes (rising or falling edges) until the minimum pulse width is exceeded. The +/- tolerance listed is the sample period (uncertainty) of the filter.
| Value | Description | Min Pulse Width | Typical Use |
|---|---|---|---|
| 0 | Unfiltered | >40ns | RS485 inputs |
| 4 | Ultra fast |
>240ns +/- 40ns |
Fast Optos |
| 1 | Fast |
>10.24 µs +/- 0.64 µs |
Fast Optos |
| 2 | Standard |
>163µs +/- 10.24µs |
Slow Optos |
| 3 | Slow |
>2.62ms +/- 0.16384ms |
Mechanical switch |
Examples
Context
See Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
|
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 4 |
| Default Value |
Depends on DIN: 4 for DIN1-2 2 for DIN3-12 |
| Data Type | Integer |
| See Also | |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
DIN1.FILTER |
3590h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIN2.FILTER |
3591h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIN3.FILTER |
3592h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
DIN4.FILTER |
3593h |
02h |
Unsigned8 |
- |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
20100 |
1 |
20100 (0x4e84) |
DIN1.FILTER |
Unsigned8 |
Read/Write |
Yes |
|
20101 |
1 |
20101 (0x4e85) |
DIN2.FILTER |
Unsigned8 |
Read/Write |
Yes |
|
20102 |
1 |
20102 (0x4e86) |
DIN3.FILTER |
Unsigned8 |
Read/Write |
Yes |
|
20103 |
1 |
20103 (0x4e87) |
DIN4.FILTER |
Unsigned8 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DIN1.FILTER |
20100 |
Unsigned8 |
Read/Write |
- |
|
DIN2.FILTER |
20101 |
Unsigned8 |
Read/Write |
- |
|
DIN3.FILTER |
20102 |
Unsigned8 |
Read/Write |
- |
|
DIN4.FILTER |
20103 |
Unsigned8 |
Read/Write |
- |